SLUSC25A February 2015 – August 2017 TPS2388
PRODUCTION DATA.
COMMAND = 16h with 1 Data Byte, Read/Write
Bit Descriptions: These bits define the timing configuration for all four ports.
Note: the PGn and PEn bits (Power Status register) are cleared when there is a TLIM, TOVLD, TMPDO, or TSTART fault condition.
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
TLIM | TSTART | TOVLD | TMPDO | ||||
R/W-0 | R/W-0 | R/W-0 | R/W-0 | R/W-0 | R/W-0 | R/W-0 | R/W-0 |
LEGEND: R/W = Read/Write; R = Read only; -n = value after reset |
Bit | Field | Type | Reset | Description | ||||
---|---|---|---|---|---|---|---|---|
7 –6 | TLIM | R/W | 0 | ILIM fault timing, which is the output current limit time duration before port turn off. This timer is active and increments to the settings defined below after expiration of the TSTART time window and when the port is limiting its output current to ILIM. If the ILIM counter is allowed to reach the programmed time-out duration specified below, the port will be powered off. The 1-second cool down timer is then started, and the port can not be turned-on until the counter has reached completion. In other circumstances (ILIM time-out has not been reached), while the port current is below ILIM, the same counter decrements at a rate 1/16th of the increment rate. The counter does not decrement below zero. The ILIM counter is also cleared in the event of a port turn off due to a Power Enable or Port Reset command, a DC disconnect event or the OSS input. Note that in the event the TLIM setting is changed while this timer is already active for a port, this timer is automatically reset then restarted with the new programmed time-out duration. Note that at the end of cool down cycle, when in semiauto mode, a detection cycle is automatically restarted if the detect enable bit is set. Also note that the cool down time count is immediately canceled with a port reset command, or if the OFF or Manual mode is selected. When a PoEPn bit in PoE Plus register is deasserted, the tLIM used for the associated port is always the nominal value (about 60 ms). If PoEPn bit is asserted, then tLIM for associated port is programmable with the following selection: |
||||
TLIM | Nominal tLIM (ms) | |||||||
0 | 0 | 60 | ||||||
0 | 1 | 15 | ||||||
1 | 0 | 12 | ||||||
1 | 1 | 10 | ||||||
5-4 | TSTART (or TINRUSH) |
R/W | 0 | START fault timing, which is the maximum allowed overcurrent time during inrush. If at the end of TSTART period the current is still limited to IInrush, the port is powered off. This is followed by a 1-second cool down period, during which the port can not be turned-on Note that at the end of cool down cycle, when in semiauto mode, a detection cycle is automatically restarted if the class and detect enable bits are set. Note that in the event the TSTART setting is changed while this timer is already active for a port, this new setting is ignored and will be applied only next time the port is turned ON. The selection is as following: |
||||
TSTART | Nominal tSTART (ms) | |||||||
0 | 0 | 60 | ||||||
0 | 1 | 30 | ||||||
1 | 0 | 120 | ||||||
1 | 1 | Reserved | ||||||
3–2 | TOVLD | R/W | 0 | ICUT fault timing, which is the overcurrent time duration before port turn off. This timer is active and increments to the settings defined below after expiration of the TSTART time window and when the port current meets or exceeds ICUT, or when it is limited by the current foldback. If the ICUT counter is allowed to reach the programmed time-out duration specified below, the port will be powered off. The 1-second cool down timer is then started, and the port can not be turned-on until the counter has reached completion. In other circumstances (ICUT time-out has not been reached), while the port current is below ICUT, the same counter decrements at a rate 1/16th of the increment rate. The counter does not decrement below zero. The ICUT counter is also cleared in the event of a port turn off due to a Power Enable or Port Reset command, a DC disconnect event or the OSS input Note that in the event the TOVLD setting is changed while this timer is already active for a port, this timer is automatically reset then restarted with the new programmed time-out duration. Note that at the end of cool down cycle, when in semiauto mode, a detection cycle is automatically restarted if the detect enable bit is set. Also note that the cool down time count is immediately canceled with a port reset command, or if the OFF or Manual mode is selected. Note that if a DCUTn bit is high in the Port Power Priority/ICUT Disable register, the ICUT fault timing for the associated port is disabled. This means that this port will not be turned off if there is only ICUT fault. The selection is as following: |
||||
TOVLD | Nominal tOVLD (ms) | |||||||
0 | 0 | 60 | ||||||
0 | 1 | 30 | ||||||
1 | 0 | 120 | ||||||
1 | 1 | 240 | ||||||
1–0 | TMPDO | R/W | 0 | Disconnect delay, which is the time to turn off a port once there is a disconnect condition, and if the dc disconnect detect method has been enabled. The TDIS counter is reset each time the current goes continuously higher than the disconnect threshold for nominally 15 ms. The counter does not decrement below zero. The selection is as following: |
||||
TMPDO | Nominal tMPDO (ms) | |||||||
0 | 0 | 360 | ||||||
0 | 1 | 90 | ||||||
1 | 0 | 180 | ||||||
1 | 1 | 720 | ||||||