SLUSCK4B September 2016 – December 2021 UCC28951-Q1
PRODUCTION DATA
The CT chosen for this design has a turns ratio (CTRAT) of 100:1 in Equation 97:
Calculate nominal peak current (IP1) at VINMIN:
The peak primary current is calculated using Equation 98:
The CS pin voltage where peak current limit will trip is:
Calculate current sense resistor (RCS) and leave 300 mV for slope compensation using Equation 100. Include a 1.1 factor for margin:
Select a standard resistor for RCS:
Estimate the power loss for RCS using Equation 102:
Calculate maximum reverse voltage (VDA) on DA using Equation 103:
Estimate the DA power loss (PDA) using Equation 104:
Calculate reset resistor R7:
Resistor R7 is used to reset the current sense transformer CT:
Resistor RLF1 and capacitor CLF form a low-pass filter for the current sense signal (Pin 15). For this design, chose the following values. This filter has a low frequency pole (fLFP) at 482 kHz, (which is appropriate for most applications) but may be adjusted to suit individual layouts and EMI present in the design.
The UCC28951-Q1 VREF output (Pin 1) needs a high frequency bypass capacitor to filter out high frequency noise. This pin needs at least 1 µF of high-frequency bypass capacitance (CREF).
The voltage amplifier reference voltage (Pin 2, EA +) can be set with a voltage divider (R1, R2), for this design example, the error amplifier reference voltage (V1) will be set to 2.5 V. Select a standard resistor value for R1 and then calculate resistor value R2.
UCC28951-Q1 reference voltage:
Set voltage amplifier reference voltage:
The voltage divider formed by resistor R3 and R4 are chosen to set the DC output voltage (VOUT) at Pin 3 (EA-).
Select a standard resistor for R3:
Calculate R4 using Equation 115:
Then choose a standard resistor for R4 using Equation 116:
TI recommends using an RCD clamp to protect the output synchronous FETs from overvoltage due to switch node ringing.