JAJSFM5 June 2018 ADS8688AT
PRODUCTION DATA.
The device uses two separate power supplies: AVDD and DVDD. The internal circuits of the device operate on AVDD; DVDD is used for the digital interface. AVDD and DVDD can be independently set to any value within the permissible range.
The AVDD supply pins must be decoupled with AGND by using a minimum 10-µF and 1-µF capacitor on each supply. Place the 1-µF capacitor as close to the supply pins as possible. Place a minimum 10-µF decoupling capacitor very close to the DVDD supply to provide the high-frequency digital switching current. The effect of using the decoupling capacitor is illustrated in the difference between the power-supply rejection ratio (PSRR) performance of the device. Figure 124 shows the PSRR of the device without using a decoupling capacitor. Figure 125 shows that the PSRR improves when the decoupling capacitors are used.
Code output near 32,769 |
Code output near 32,768 |