JAJSR80 September 2023 AMC131M01
PRODUCTION DATA
Multiple registers are read from the device when nnn nnnn is specified as a number greater than zero in the RREG command word. As with all SPI commands on the AMC131M01, the response occurs on the output in the frame following the command. Instead of a single acknowledgment word, the response spans multiple words to shift out all requested registers. Continue toggling SCLK to accommodate outputting the entire data stream. ADC conversion data are not output in the frame following an RREG command to read multiple registers. Figure 8-23 shows an example of reading multiple registers.