JAJSH89D May 2012 – April 2019 CDCUN1208LP
PRODUCTION DATA.
Table 6 describes how to set the input divider using the DIVIDE pin. If the /8 setting is desired, then this feature is accessed through the host configuration method only; refer to Device Control Using the Host Interface.
DIVIDE (Pin 1) | INDIV DIVIDER SETTING |
---|---|
LOW | /2 |
HIGH | /4 |
OPEN | /1 |