JAJSC33G February 2015 – October 2022 DP83867CR , DP83867IR
PRODUCTION DATA
デバイスごとのパッケージ図は、PDF版データシートをご参照ください。
BIT | BIT NAME | DEFAULT | DESCRIPTION |
---|---|---|---|
15:8 | TDR_PEAKS_LOC_D_4 | 0, RO | Location of the fifth peak discovered by the TDR mechanism on channel D. The value of these bits is translated into distance from the PHY. |
7:0 | TDR_PEAKS_LOC_D_3 | 0, RO | Location of the fourth peak discovered by the TDR mechanism on channel D. The value of these bits is translated into distance from the PHY. |