JAJSH73B April 2019 – July 2021 INA186
PRODUCTION DATA
The INA186 is in normal operation when the following conditions are met:
For devices that do not feature a REF pin that value for VREF will be zero. During normal operation, this device produces an output voltage that is the amplified representation of the difference voltage from IN+ to IN– plus the voltage applied to the REF pin.