JAJSFI3A May 2018 – November 2018 TAS3251
PRODUCTION DATA.
The following diagram shows an application using pre-filter PBTL, which requires only two inductors. Note that the inductor should have a saturation current that is equal to the maximum current during an output short condition.