JAJSPM4A September 2016 – February 2023 TCA6408A-Q1
PRODUCTION DATA
In the event of a glitch or data corruption, TCA6408A-Q1 can be reset to its default conditions by using the power-on reset feature. Power-on reset requires that the device go through a power cycle to be completely reset. This reset also happens when the device is powered on for the first time in an application.
Ramping up the device VCCP before VCCI is recommended to prevent SDA from potentially being stuck LOW.
The two types of power-on reset are shown in Figure 9-6 and Figure 9-7.
Table 9-1 specifies the performance of the power-on reset feature for TCA6408A-Q1 for both types of power-on reset.
PARAMETER | MIN | TYP | MAX | UNIT | ||
---|---|---|---|---|---|---|
tFT | Fall rate | See Figure 9-6 | 0.1 | 2000 | ms | |
tRT | Rise rate | See Figure 9-6 | 0.1 | 2000 | ms | |
tRR_GND | Time to re-ramp (when VCCP drops to GND) | See Figure 9-6 | 1 | μs | ||
tRR_POR50 | Time to re-ramp (when VCCP drops to VPOR_MIN – 50 mV) | See Figure 9-7 | 1 | μs | ||
VCCP_GH | Level that VCCP can glitch down from VCCP, but not cause a functional disruption when tVCCP_GW = 1 μs | See Figure 9-8 | 1.2 | V | ||
VCCP_MV | The minimum voltage that VCC can glitch down to without causing a reset (VCC_GH must not be violated) | See Figure 9-8 | 1.5 | V | ||
tVCCP_GW | Glitch width that does not cause a functional disruption when tVCCP_GH = 0.5 × VCCx | See Figure 9-8 | 10 | μs | ||
VPORF | Voltage trip point of POR on falling VCCP | 0.6 | 1 | V | ||
VPORR | Voltage trip point of POR on rising VCCP | 1.2 | 1.5 | V |
Glitches in the power supply can also affect the power-on reset performance of this device. The glitch width (tVCCP_GW) and height (VCCP_GH) are dependent on each other. The bypass capacitance, source impedance, and device impedance are factors that affect power-on reset performance. Figure 9-8 and Table 9-1 provide more information on how to measure these specifications.
VPOR is critical to the power-on reset. VPORR / VPORF is the voltage level at which the reset condition is released/asserted and all the registers and the I2C/SMBus state machine are initialized to the default states (upon a release of a reset condition). The voltage that the device has a reset condition asserted or released differs based on whether VCCP is being lowered to or from 0. Figure 9-9 and Table 9-1 provide more details on this specification.