JAJSGF6D May 2015 – January 2020 TMP107
PRODUCTION DATA.
The register pointer phase is provided only if the communication is an address operation. This phase of the communication shows the register pointer of the device that the host in going to write to or read from. The pointer byte has special identification code bits, as shown in Figure 21.