JAJSGF6D May 2015 – January 2020 TMP107
PRODUCTION DATA.
The configuration register is a read and write register used to store bits that control the part operation. The format and power-up or reset value of the configuration register for the TMP107 is shown in Figure 32 and Table 5. When the NUS bit is 0, all writes to this register are stored in register logic. When NUS is 1, then all writes to this register program the EEPROM location that stores the configuration bits. Writes to this location are followed by a 16-ms wait period for programming the EEPROM. When the configuration register is written, the current conversion is aborted and new action is taken based on the new written bits. Thus, if the TMP107 is put into shutdown, the device goes into shutdown immediately. If the conversion rate is changed, any ongoing conversion is aborted and a new conversion starts with the new conversion rate.
15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
CR2 | CR1 | CR0 | OS | SD | FH1 | FL1 | T1/A1 |
R/W-5h | R/W-0h | R/W-0h | R-0h | R-0h | R/W-0h | ||
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
POL1 | FH2 | FL2 | T2/A2 | POL2 | Reserved | RST | Reserved |
R/W-0h | R-0h | R-0h | R/W-0h | R/W-0h | R-0h | W-0h | R-0h |
LEGEND: R/W = Read/Write; R = Read only; W = Write only; -n = value after reset |
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
15-13 | CR2-CR0 | R/W | 5h | Conversion rate.
The conversion rate bits control the update rate of the analog-to-digital converter (ADC). Table 6 describes the relationship between the values of the conversion rate bits and the corresponding conversion time and average quiescent current. These bits only affect continuous-conversion mode and not one-shot mode. |
12 | OS | R/W | 0h | One-shot mode.
0: Default. 1: Starts a single temperature conversion if the SD bit is set to 1. The TMP107 returns to the shutdown state at the completion of the single conversion. When the configuration register is read, OS always reads zero. |
11 | SD | R/W | 0h | Shutdown mode.
0: The TMP107 is in continuous-conversion mode. 1: The TMP107 is in shutdown mode. Initiate a conversion by writing a 1 to the OS bit. |
10 | FH1 | R | 0h | High limit 1 flag.
0: Indicates that the temperature result does not exceed high limit 1. 1: Indicates when the temperature result exceeds high limit 1. |
9 | FL1 | R | 0h | Low limit 1 flag. In therm mode, this bit is not used and always reads 0.
0: In alert mode, this bit indicates that the temperature result is greater than low limit 1. 1: In alert mode, this bit indicates when the temperature result is less than low limit 1. |
8 | T1/A1 | R/W | 0h | Alert and therm mode 1.
0: Alert mode: In this mode, the high limit 1 and low limit 1 form a window. If the temperature result is greater than high limit 1 or less than low limit 1, the respective flag (either FH1 or FL1) is asserted. After the flag is asserted, clear the flag by reading the configuration register. 1: Therm mode: In this mode, the limits are used to form an upper limit threshold detector. If the temperature result is greater than high limit 1, the FH1 flag is asserted. The FH1 flag is then deasserted only after the temperature drops below low limit 1. In therm mode, only the FH1 flag is active. The FL1 flag always reads 0. In this mode, the flags are asserted and deasserted only at the end of a conversion and cannot be cleared by a configuration register read. |
7 | POL1 | R/W | 0h | 0: Polarity of the ALERT1 pin is active low.
1: Polarity of the ALERT1 pin is active high. |
6 | FH2 | R | 0h | High limit 2 flag.
0: Indicates that the temperature result does not exceed high limit 2. 1: Indicates when the temperature result exceeds high limit 2. |
5 | FL2 | R | 0h | Low Limit 2 Flag. In therm mode, this bit is not used and always reads 0.
0: In alert mode, this bit indicates that the temperature result is greater than low limit 2. 1: In alert mode, this bit indicates when the temperature result is less than low limit 2. |
4 | T2/A2 | R/W | 0h | Alert and therm mode 2.
0: Alert mode: in this mode, the high limit 2 and low limit 2 form a window. If the temperature result is greater than high limit 2 or less than low limit 2, the respective flag (either FH2 or FL2) is asserted. After the flag is asserted, clear the flag by reading the configuration register. 1: Therm mode: in this mode, the limits are used to form an upper limit threshold detector. If the temperature result is greater than high limit 2, the FH2 flag is asserted. The FH2 flag is then deasserted only after the temperature drops below low limit 2. In therm mode, only the FH2 flag is active. The FL2 flag always reads 0. In this mode, the flags are asserted and deasserted only at the end of a conversion and cannot be cleared by a configuration register read. |
3 | POL2 | R/W | 0h | 0: Polarity of the ALERT2 pin is active low.
1: Polarity of the ALERT2 pin is active high. |
2 | Reserved | R | 0h | Reserved |
1 | RST | W | 0h | Software reset.
0: Default. 1: Reset. This bit is a write-only bit and is used to perform a software reset on the TMP107. |
0 | Reserved | R/W | 0h | Reserved |
CR2 | CR1 | CR0 | CONVERSION PERIOD | CONVERSIONS PER SECOND | AVERAGE IQ
(V+ = 3.3 V) |
---|---|---|---|---|---|
0 | 0 | 0 | 15 ms | 62 | 200 µA |
0 | 0 | 1 | 50 ms | 20 | 20 µA |
0 | 1 | 0 | 100 ms | 10 | 15 µA |
0 | 1 | 1 | 250 ms | 4 | 11 µA |
1 | 0 | 0 | 500 ms | 2 | 9 µA |
1 | 0 | 1 | 1 s (default) | 1 (default) | 7 µA |
1 | 1 | 0 | 4 s | 0.25 | 6 µA |
1 | 1 | 1 | 16 s | 0.0625 | 5 µA |