JAJSSJ8 December 2023 TPS281C100
PRODUCTION DATA
The diagnostic enable pin, DIAG_EN, offers multiplexing of the microcontroller diagnostic input for current sense or digital status, by sharing the same sense resistor and ADC line or I/O port among multiple devices.
In addition, this pin can be used to manage power dissipation by the device. During the ouput-on period, if no continious sense output diagnositcs are required, the diagnostic disable feature will lower the operating current. On the other hand, the output-off period, the diagnostic disable function lowers the current consumption for the standby condition.