JAJSHA7C February 2018 – February 2020 TPS2HB16-Q1
PRODUCTION DATA.
The TPS2HB16-Q1 is designed to operate in the automotive environment. The protection mechanisms allow the device to be robust against many system-level events such as load dump, reverse battery, short-to-ground, and more.
There are two protection features which, if triggered, will cause the switch to automatically disable:
When any of these protections are triggered, the device will enter the FAULT state. In the FAULT state, the fault indication will be available on the SNS pin (see the Diagnostic Mechanisms section of the data sheet for more details). For version F of the device, the fault will also be indicated on the FLT1 or FLT2 pin, depending on the channel that recognizes the fault.
The switch is no longer held off and the fault indication is reset when all of the below conditions are met:
NOTE
CH1 and CH2 operate independently. If there is a fault on one channel, the other channel is not affected. On version F of the device, FLT1 and FLT2 each independently diagnose each channel output.