JAJSIY9D March 2020 – October 2020 TPS63900
PRODUCTION DATA
The device turns on when all the following conditions are true:
The device turns off when at least one of the following conditions is true:
A complete state diagram is shown in Figure 7-13.
After the device turns on, the internal reference system starts, then the trimming information and the CFG pins are read out. The device ignores any further changes to the CFG pins during device operation.
Figure 7-5 shows the internal start-up sequence.