The DLP5532HBQ1EVM
comes with onboard serial Flash that is pre-programmed with software and basic
configuration. The software and configuration can be updated by reprogramming the serial
Flash with the DLPC230-Q1 Automotive Control Program. Steps to re-program the serial Flash
are listed below.
- Using the DLPC230-Q1 Automotive Control Program, that is connected to the EVM,
navigate to the Flash Program tab.
- Navigate to the Read Flash sub
tab and select entire flash content to be saved to a local storage location.
(Note that this step is optional but highly recommended to save the current flash
content as a backup.
- Navigate back to the Program Flash sub tab and using the folder icon,
select an Image File (.bin) and open it.
- Click Program and Verify Flash Memory.
Note that if the device is in Display mode, it is
automatically be switched to Standby during programming.