JAJSAC1G November 2007 – November 2023 LM3481
PRODUCTION DATA
Proper selection of the inductors L1 and L2 to maintain constant current mode requires calculations of the following parameters.
Average current in the inductors:
Peak-to-peak ripple current, to calculate core loss if necessary:
Maintaining the condition IL > ΔIL/2 to ensure continuous conduction mode yields the following minimum values for L1 and L2:
Peak current in the inductor, to ensure the inductor does not saturate:
IL1PK must be lower than the maximum current rating set by the current sense resistor.
The value of L1 can be increased above the minimum recommended value to reduce input ripple and output ripple. However, once ΔIL1 is less than 20% of IL1AVE, the benefit to output ripple is minimal.
By increasing the value of L2 above the minimum recommendation, ΔIL2 can be reduced, which in turn will reduce the output ripple voltage:
where ESR is the effective series resistance of the output capacitor.
If L1 and L2 are wound on the same core, then L1 = L2 = L. All the equations above will hold true if the inductance is replaced by 2L.