JAJSFY8A August 2018 – November 2018 ADS1119
PRODUCTION DATA.
The serial clock (SCL) line is used to clock data in and out of the device. The master always drives the clock line. The ADS1119 cannot act as a master and as a result can never drive SCL.
The serial data (SDA) line allows for bidirectional communication between the host (the master) and the ADS1119 (the slave). When the master reads from a ADS1119, the ADS1119 drives the data line; when the master writes to a ADS1119, the master drives the data line.
Data on the SDA line must be stable during the high period of the clock. The high or low state of the data line can only change when the SCL line is low. One clock pulse is generated for each data bit transferred. When in an idle state, the master should hold SCL high.