JAJU680A January 2019 – July 2022
Variation of the absolute time of flight (AbsToF) measurements is also an important metric in both flow meter applications as well as other applications like mixture analysis. The important metric in the case of AbsToF is also the drift over time as well as the standard deviation of the measurements. As can be seen from the figure below, the AbsToF is inversely proportional to temperature (it increases as temperature decreases). The standard deviation in AbsToF was found to be approximately 30 ns across various transducer pairs.