SBAA400A September   2019  – December 2023 PCM5140-Q1 , PCM6140-Q1 , TLV320ADC5140 , TLV320ADC6140

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
  5. 2Dynamic Range Enhancer
    1. 2.1 High Pass Filter
    2. 2.2 DRE Parameters
    3. 2.3 Sample Rate Support
  6. 3Example
  7. 4References
  8. 5Revision History

Dynamic Range Enhancer

Figure 2-1 shows the signal processing chain for TLV320ADC5140, TLV320ADC6140, PCM5140-Q1, and PCM6140-Q1 devices. The dynamic range performance of the front-end PGA in TLV320ADC5140/PCM5140-Q1 and TLV320ADC6140/PCM6140-Q1 devices are 120 dB and 122 dB respectively. The subsequent delta-sigma ADC has 108 dB dynamic range for the TLV320ADC5140/PCM5140-Q1 and 113 dB dynamic range for the TLV320ADC6140/PCM6140-Q1. Without the DRE, the ultra-low noise performance of the PGA is limited by the ADC performance and the overall channel dynamic range is determined by the dynamic range of the ADC. With the DRE, the overall channel dynamic range can be improved beyond the dynamic range of the ADC and is limited more by the dynamic range of the PGA.

GUID-E5A5226F-C16A-4D35-914B-FB4085CB657B-low.pngFigure 2-1 Signal Processing Block Diagram

The DRE algorithm monitors the input signal and increases the gain of the analog PGA for signal levels below a threshold. At the same time, the DRE algorithm creates a corresponding reciprocal attenuation in the digital circuits so the net effect of the analog PGA gain and digital attenuation cancel each other out. Thus the DRE improves the dynamic range without increasing the overall channel gain. The DRE does not gain signals above the threshold. Boosting the low-level signals in analog keeps the input to the ADC significantly above its noise floor and thus prevents the ADC performance from being the limiting factor. Subsequent processing is done using a high-performance, 32-bit, digital signal processor with very low quantization noise, and, therefore, the PGA performance becomes the limiting factor in the overall channel performance.

TLV320ADC5140, TLV320ADC6140, PCM5140-Q1, and PCM6140-Q1 devices support up to four analog input channels. All analog input channels support DRE. The devices support differential or single-ended signals from an analog microphone source or auxiliary line input. The analog microphone inputs support electret condenser and microelectrical-mechanical (MEMS) microphones. Even though the devices also support digital pulse density modulated (PDM) digital microphones, the DRE does not support the digital channels as the analog gain of the digital microphone cannot be controlled.

The TLV320ADCx140/PCMx140-Q1 family of devices also support an automatic gain control (AGC) algorithm on the analog channels to maintain a constant nominal output level. AGC and DRE algorithms cannot be used simultaneously since both the algorithms control the PGA. DRE or AGC selection is done using AGC_DRE_SEL field of DSP_CFG1 register (page = 0x00, address = 0x6C) as shown in Table 2-1.

Table 2-1 DRE Selection Using DSP_CFG1 Register
BITFIELDTYPERESETDESCRIPTION
3AGC_DRE_SELR/W0hDRE or DRE selection when is enabled for any channel.
0d = DRE is selected.
1d = DRE is selected.

DRE can be independently enabled or disabled for each channel using the following register bits:

  • CH1_DREEN (P0_R60_D0)
  • CH2_DREEN (P0_R65_D0)
  • CH3_DREEN (P0_R70_D0)
  • CH4_DREEN (P0_R75_D0)