SBAU420 March 2023
Each 3D Hall-effect sensor is fabricated on a die and the package assembly has these dies stacked vertically for a minimal offset in the XY plane. Device tolerances for sensitivity gain and offset should be canceled out:
After correction sensitivity and offset errors of the device, the sensors may still experience some measurement error due to mechanical rotations of the package relative to the rotating magnet. The most straightforward alignment method is achieved by placing the sensor on-axis to the rotating magnet.
In an ideal on-axis placement, the X and Y axis data will observe a decrease in magnitude only, with no impact to observed angle linearity. As the package is mechanically offset, peak input data for X and Y axes will vary, and the severity of amplitude correction needed will become more significant. Additionally, package rotations may cause angle offset relative to the position of the magnet or phase error between the observed X and Y axis input. This happens as each sensing element detects the field which is orthogonal to the sensing element and the sensor is no longer orthogonal to the rotating magnet. As a result, each sensing element detects a portion of the vector component from either of the other two axes. This error may vary based on the installation of either the magnet or sensor within the system. Often, end-of-line calibration for each sensor is required after full system assembly to achieve the best results. For more information, refer to the Texas Instruments Achieving Highest System Angle Sensing Accuracy application note.