SBOA564 December 2022 TRF0206-SP
The TRF0206-SP is packaged in a 12-pin, thermally-enhanced, leadless ceramic chip carrier package (LCCC) as shown in Figure 3-1. The TRF0206-SP Radiation Board was used to evaluate the single-events-effects (SEE) of the TRF0206-SP. Top view of the evaluation board used for the radiation testing are shown in Figure 3-1. Schematic of the evaluation board used for radiation testing is shown in Figure 3-2. For more technical information about the TRF0206-SP, see https://www.ti.com/product/TRF0206-SP/technicaldocuments.