SBVS083E January 2007 – January 2015
PRODUCTION DATA.
An evaluation module (EVM) is available to assist in the initial circuit performance evaluation using the TPS780. The TPS780XXEVM-301 evaluation module (and related user's guide) can be requested at the Texas Instruments website through the product folders or purchased directly from the TI eStore.
Computer simulation of circuit performance using SPICE is often useful when analyzing the performance of analog circuits and systems. A SPICE model for the TPS780 series is available through the product folders under Tools & Software.
PRODUCT | VOUT |
---|---|
TPS780vvvxxxyyyz | vvv is the nominal output voltage for VOUT(HI) and corresponds to VSET pin low. xxx is the nominal output voltage for VOUT(LO) and corresponds to VSET pin high. yyy is the package designator. z is the tape and reel quantity (R = 3000, T = 250). Adjustable version(3)(4) |
MSP430 is a trademark of TI.
All other trademarks are the property of their respective owners.
These devices have limited built-in ESD protection. The leads should be shorted together or the device placed in conductive foam during storage or handling to prevent electrostatic damage to the MOS gates.
SLYZ022 — TI Glossary.
This glossary lists and explains terms, acronyms, and definitions.