SCEU028 November   2023

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
    1. 1.1 Kit Contents
    2. 1.2 Features
  5. 2Hardware
    1. 2.1 PCB Overview
    2. 2.2 Hardware Setup
  6. 3Bill of Materials
  7. 4Revision History

Hardware Setup

Programmer Hardware Connections

The TPLD-PROGRAM was designed to interface with a computer using a USB-to-Micro USB cable and to a TPLD EVM using a 14-position cable. Both cables are included in the kit for the TPLD-PROGRAM. If either of the cables is lost or damaged, TI recommends ordering new cables using the Digi-Key part number included on the kit list provided. Using other connectors could damage the boards or other connected equipment.

GUID-20231017-SS0I-QKP2-DP1X-44FWRGXFSSF0-low.svg Figure 2-3 TPLD-PROGRAM Hardware Connections

Programmer Case Construction

The cases for the TPLD-PROGRAM are designed to easily snap together. To reconstruct a programmer case that has been disassembled, follow these steps.

GUID-20231004-SS0I-GGXM-0FTK-RRXQNGJV3D86-low.svg Figure 2-4 TPLD-PROGRAM Case Assembly
  1. Insert the light diffuser into the case cover, lining up arrow and LED cutouts.
  2. Place the programmer flat in the base, using LED cutouts to align the TPLD-PROGRAM and the case.
  3. Snap the cover onto the base, aligning 14-Pin header with the cutout in the case.