SCPA071 February 2024 SN3257-Q1 , TMUX1308-Q1
In the automotive industry, particularly in EV/HEV applications, it is crucial to limit the effects that arise as a result of I/O signals shorting to the battery voltage, VBAT. This is commonly referred to as Short to Battery protection. One way to achieve this protection is by implementing external diode and resistor networks as shown in Figure 1-1 to keep the input signals within the supply voltage. Alternatively, choosing a device with Injection Current Control circuitry as highlighted in Figure 2-1 eliminates the need for extensive external components to achieve such protection.