SFFS263 October   2021 INA301-Q1

 

  1.   Trademarks
  2. 1Overview
  3. 2Functional Safety Failure In Time (FIT) Rates
  4. 3Failure Mode Distribution (FMD)
  5. 4Pin Failure Mode Analysis (Pin FMA)

Pin Failure Mode Analysis (Pin FMA)

This section provides a Failure Mode Analysis (FMA) for the pins of the INA301-Q1. The failure modes covered in this document include the typical pin-by-pin failure scenarios:

  • Pin short-circuited to Ground (see Table 4-2)
  • Pin open-circuited (see Table 4-3)
  • Pin short-circuited to an adjacent pin (see Table 4-4)
  • Pin short-circuited to Supply (see Table 4-5)

Table 4-2 through Table 4-5 also indicate how these pin conditions can affect the device as per the failure effects classification in Table 4-1.

Table 4-1 TI Classification of Failure Effects
ClassFailure Effects
APotential device damage that affects functionality
BNo device damage, but loss of functionality
CNo device damage, but performance degradation
DNo device damage, no impact to functionality or performance

Figure 4-1 shows the INA301-Q1 pin diagram. For a detailed description of the device pins please refer to the Pin Configuration and Functions section in the INA301-Q1 data sheet.

GUID-20210902-SS0I-DSDJ-KWG9-P9SK7VGKGFMP-low.gif Figure 4-1 Pin Diagram

Following are the assumptions of use and the device configuration assumed for the pin FMA in this section:

  • TA = -40°C to +125°C
  • VS = 5 V
  • VIN+ = 12 V
  • REF = VS/2.
Table 4-2 Pin FMA for Device Pins Short-Circuited to Ground
Pin NamePin No.Description of Potential Failure Effect(s)Failure Effect Class
VS1Power supply shorted to ground.B
OUT2Output shorts to ground. When left in this configuration for a long time, under high supplies self heating could cause dice junction temperature to exceed 150 degrees Celsius.B
LIMIT3ALERT output is stuck low.B
GND4Normal Operation.D
RESET5If intended connection is not GND, functionality will be affected.D if RESET=GND by design; C otherwise
ALERT6ALERT output is stuck low.B
IN-7In high-side configuration, a short from the bus supply to GND will occur. High current will flow from bus supply to ground. In low-side configuration, normal operation.B for high-side or D for low-side
IN+8In high-side configuration, a short from the bus supply to GND will occur. High current will flow from bus supply to ground. In low side configuration, input pins are shorted.B
Table 4-3 Pin FMA for Device Pins Open-Circuited
Pin NamePin No.Description of Potential Failure Effect(s)Failure Effect Class
VS1No power supply to device. Device may be biased through inputs. Output will be close to GND.B
OUT2Output can be left open, there is no effect on the IC.D
LIMIT3Comparator threshold is not defined.B
GND 4 Output will be incorrect as it is no longer referenced to GND. B
RESET5Comparator mode is not defined.B
ALERT6Pin can be left open if not needed.D
IN-7Differential input voltage is not well defined.B
IN+8Differential input voltage is not well defined.B
Table 4-4 Pin FMA for Device Pins Short-Circuited to Adjacent Pin
Pin NamePin No.Shorted toDescription of Potential Failure Effect(s)Failure Effect Class
VS1OUTOutput shorts to supply. When left in this configuration for a long time, under high supplies self heating could cause dice junction temperature to exceed 150 degrees Celsius.B
OUT2LIMITComparator output will be unpredictable.B
LIMIT3GNDALERT output is stuck low.B
GND4RESETIf intended connection is not GND, functionality will be affected.D if RESET=GND by design; C otherwise
RESET5ALERTALERT Comparator output will be unpredictable.B
ALERT6IN-In low-side configuration, ALERT output is stuck low; In high-side configuration, device damage is possible.C for low-side; A for high-side
IN-7IN+Input differential voltage=0V.C
IN+8VSIn high-side configuration, a short from the bus supply to VS will occur. High current will flow from bus supply to VS or vice versa. Device could be damaged.A
Table 4-5 Pin FMA for Device Pins Short-Circuited to Supply
Pin NamePin No.Description of Potential Failure Effect(s)Failure Effect Class
VS1Normal operation.D
OUT2Output shorts to supply. When left in this configuration for a long time, under high supplies self heating could cause dice junction temperature to exceed 150 degrees Celsius.B
LIMIT3ALERT is stuck high or unpredictable.B
GND4Power supply shorted to GND.B
RESET5Comparator1 in Latch mode. D if RESET=VS by design; C otherwise
ALERT6ALERTis stuck high. Power supply could be shorted to GND though this pin.A
IN-7In high-side configuration, a short from the bus supply to VS will occur. High current will flow from bus supply to VS or vice versa. Device could be damaged.A for High side or B for low side
IN+8In high-side configuration, a short from the bus supply to VS will occur. High current will flow from bus supply to VS or vice versa. Device could be damaged.A for High side or B for low side