SFFS638 December   2023 TPS4800-Q1

 

  1.   1
  2.   Trademarks
  3. 1Overview
  4. 2Functional Safety Failure In Time (FIT) Rates
  5. 3Failure Mode Distribution (FMD)
  6. 4Pin Failure Mode Analysis (Pin FMA)

Pin Failure Mode Analysis (Pin FMA)

This section provides a Failure Mode Analysis (FMA) for the pins of the TPS4800-Q1. The failure modes covered in this document include the typical pin-by-pin failure scenarios:

  • Pin short-circuited to Ground (see Table 4-2)
  • Pin open-circuited (see Table 4-3)
  • Pin short-circuited to an adjacent pin (see Table 4-4)
  • Pin short-circuited to supply (see Table 4-5)

Table 4-2 through Table 4-5 also indicate how these pin conditions can affect the device as per the failure effects classification in Table 4-1.

Table 4-1 TI Classification of Failure Effects
ClassFailure Effects
APotential device damage that affects functionality
BNo device damage, but loss of functionality
CNo device damage, but performance degradation
DNo device damage, no impact to functionality or performance

Figure 4-1 shows the TPS4800-Q1 pin diagram. For a detailed description of the device pins please refer to the Pin Configuration and Functions section in the TPS4800-Q1 data sheet.

GUID-20231106-SS0I-L4GQ-TQ1C-LKGFQKZCNMQH-low.svg Figure 4-1 Pin Diagram

Following are the assumptions of use and the device configuration assumed for the pin FMA in this section:

  • Follow data sheet recommendation for operating conditions, external component selection and PCB layout
Table 4-2 Pin FMA for Device Pins Short-Circuited to Ground
Pin Name Pin No. Description of Potential Failure Effect(s) Failure Effect Class
EN/UVLO 1 Normal operation. The device is disabled. B
OV 2 Normal operation. Overvoltage functionality is disabled. B
INP 3 Normal operation. The PD output is low and the external FET is off. B
FLT_GD 4 Charge pump UVLO fault diagnostic cannot be reported. B
FLT 5 Overcurrent, UVLO fault diagnostic cannot be reported. B
GND 6 Normal operation D
CS_SEL 7 Normal operation with current sensing configured for high side sensing. B
ISCP

8

SCP threshold sets to minimum threshold. B
TMR 9 Overcurrent does not get detected hence overcurrent protection is disabled. B
SCP_TEST 10 Normal operation. B
N.C 11 No effect. Normal operation. D
BST 12 Gate Driver supply does not come up. FETs remain OFF. B
SRC 13 Short to GND protection kicks in. B
PD 14 With PD grounded, if the pin voltage between SRC and PD exceeds the pin data sheet range, it can cause device damage due to voltage breakdown on ESD circuit. A
PU 15 Gate Driver supply gets short circuited. FETs remain OFF. B
CS- 17 Short to GND protection kicks in. B
CS+ 18 With CS+ grounded, if the pin voltage between CS+ and CS– exceeds the pin data sheet range, it can cause device damage due to voltage breakdown on ESD circuit. A
N.C 19 Normal operation. D
VS 20 Device supply grounded. Device does not power up. B
Table 4-3 Pin FMA for Device Pins Open-Circuited
Pin Name Pin No. Description of Potential Failure Effect(s) Failure Effect Class
EN/UVLO 1 Internal pulldown brings EN/UVLO to low disabling the device. B
OV 2 Internal pulldown brings OV to low. Overvoltage functionality is disabled. B
INP 3 Internal pulldown brings INP to low, pulling PD output low. B
FLT_GD 4 Charge pump UVLO fault diagnostic cannot be reported. B
FLT 5 Overcurrent, UVLO fault diagnostic cannot be reported. B
GND 6 Device does not power up and is disabled. B
CS_SEL 7 Internal pulldown brings CS_SEL to low, resulting in normal operation with current sensing configured for high side sensing. B
ISCP 8 SCP threshold sets to maximum threshold. B
TMR 9 Overcurrent response time and auto-retry duration gets reduced to device minimum setting. C
SCP_TEST 10 Internal pulldown brings CS_SEL to low, resulting in normal operation. B
N.C 11 No effect. Normal operation. D
BST 12 External FET can get turned ON and OFF repetitively due to no capacitor connection at BST pin. B
SRC 13 The external FET does not turned OFF as the FET source got disconnected from the internal pulldown driver. B
PD 14 The external FET does not turn OFF as the FET GATE disconnects from the internal pulldown driver. B
PU 15 The external FET does not turn OFF as the FET GATE disconnects from the internal pulldown driver. B
CS- 17 CS- gets internally clamped to CS+ minus 2 diode drops. If ISCP feature is used, then the external FET may not turn ON due to false over current detection. B
CS+ 18 ISCP feature will not work. B
N.C 19 Normal operation. D
VS 20 Device does not get powered up and is disabled. B
Table 4-4 Pin FMA for Device Pins Short-Circuited to Adjacent Pin
Pin Name Pin No. Shorted to Description of Potential Failure Effect(s) Failure Effect Class
EN/UVLO 1 2 (OV) If EN/UVLO is driven high then OV also gets detected high making the device PD pulled low to SRC and external FET gets disabled. B
OV 2 3 (INP) If INP is driven high then OV also gets detected high making the device PD pulled low to SRC and external FET gets disabled. B
INP 3 4 (FLT_GD) Charge pump UVLO fault diagnostic cannot be reported. B
FLT_GD 4 5 (FLT) Overcurrent, UVLO, Charge pump UVLO fault diagnostic cannot be reported. B
FLT 5 6 (GND) Overcurrent, UVLO fault diagnostic cannot be reported. B
GND 6 7 (CS_SEL) Normal operation. Device gets configured for high side sensing. B
CS_SEL 7 8 (ISCP) With CS_SEL grounded then SCP threshold sets to minimum threshold. With CS_SEL pulled high then SCP threshold sets to maximum threshold. C
ISCP 8 9 (TMR) TMR and ISCP thresholds get affected. External FET shuts off at a different threshold than set by ISCP. During an overcurrent fault the device is in Latch-off mode if ISCP has a < 100 kΩ resistor. C
TMR 9 10 (SCP_TEST) SCP_TEST feature gets disabled. B
N.C 11 12 (BST) No effect. Normal operation. D
BST 12 13 (SRC) Gate drive supply gets shorted and external FETs do not turn ON. B
SRC 13 14 (PD) Shorting of the pulldown switch (between PD and SRC) of the internal gate driver. External FET remains OFF. B
PD 14 15 (PU) Turn ON and OFF speeds of the external FETs can get impacted. C
CS- 17 18 (CS+) Bypasses the external current sense resistor or FET VDS sensing based on application circuit. SCP features get disabled. B
CS+ 18 19 (N.C) Normal operation. D
N.C 19 20 (VS) Normal operation. D
Table 4-5 Pin FMA for Device Pins Short-Circuited to supply
Pin Name Pin No. Description of Potential Failure Effect(s) Failure Effect Class
EN/UVLO 1 EN/UVLO pin is supply rated. Device remains enabled. B
OV 2 OV pin is supply rated. PD remains pulled low to SRC due to overvoltage fault. B
INP 3 INP pin is supply rated and will be treated driven high. B
FLT_GD 4 If pin voltage exceeds the pin data sheet range, it can cause device damage due to voltage breakdown on ESD circuit. A
FLT 5 If pin voltage exceeds the pin data sheet range, it can cause device damage due to voltage breakdown on ESD circuit. A
GND 6 Supply power is bypassed and device does not turn on. B
CS_SEL 7 CS_SEL pin is supply rated. Device gets configured for low side current sensing. B
ISCP 8 If pin voltage exceeds the pin data sheet range, it can cause device damage due to voltage breakdown on ESD circuit. A
TMR 9 If pin voltage exceeds the pin data sheet range, it can cause device damage due to voltage breakdown on ESD circuit. A
SCP_TEST 10 If pin voltage exceeds the pin data sheet range, it can cause device damage due to voltage breakdown on ESD circuit. A
N.C 11 If pin voltage exceeds the pin data sheet range, it can cause device damage due to voltage breakdown on ESD circuit. A
BST 12 If pin voltage exceeds the pin data sheet range, it can cause device damage due to voltage breakdown on ESD circuit. A
SRC 13 Output stuck on to supply B
PD 14 If pin voltage exceeds the pin data sheet range, it can cause device damage due to voltage breakdown on ESD circuit. A
PU 15 If pin voltage exceeds the pin data sheet range, it can cause device damage due to voltage breakdown on ESD circuit. A
CS- 17 In the application, the external sense resistor or FET VDS sensing gets bypassed. short circuit protection will not work. A
CS+ 18 No effect. Normal operation. D
N.C 19 No effect. Normal operation. D
VS 20 No effect. Normal operation. D