SFFS790 February   2024 TXV0108-Q1

 

  1.   1
  2.   Trademarks
  3. 1Overview
  4. 2Functional Safety Failure In Time (FIT) Rates
  5. 3Failure Mode Distribution (FMD)
  6. 4Pin Failure Mode Analysis (Pin FMA)

Pin Failure Mode Analysis (Pin FMA)

This section provides a Failure Mode Analysis (FMA) for the pins of the TXV0108-Q1 (VQFN package). The failure modes covered in this document include the typical pin-by-pin failure scenarios:

Table 4-2 through Table 4-6 also indicate how these pin conditions can affect the device as per the failure effects classification in Table 4-1.

Table 4-1 TI Classification of Failure Effects
ClassFailure Effects
APotential device damage that affects functionality
BNo device damage, but loss of functionality
CNo device damage, but performance degradation
DNo device damage, no impact to functionality or performance

Pin Diagram (VQFN) Package shows the TXV0108-Q1 pin diagram for the VQFN package. For a detailed description of the device pins please refer to the Pin Configuration and Functions section in the TXV0108-Q1 data sheet.

Figure 4-1 Pin Diagram (VQFN) Package

Following are the assumptions of use and the device configuration assumed for the pin FMA in this section:

Table 4-2 Pin FMA for Device Pins Short-Circuited to Ground
Pin NamePin No.Description of Potential Failure Effect(s)Failure Effect Class
VCCA1GND short to VCC, device will be bypassed - may cause system damage, but not device damageB
DIR2Direction control will fixed, B --> A direction.B
A1 - A83 to 10If configured as an output then damage is possible. If configured as input, no damage, but output will not switch.A
GND11 to 13Normal operation.D
B8 - B114 to 21If configured as an output then damage is possible. If configured as input, no damage, but output will not switch.A
OE (active low)22Outputs will remain enabled.B
VCCB23 to 24GND short to VCC, device will be bypassed - may cause system damage, but not device damage.B
Table 4-3 Pin FMA for Device Pins Open-Circuited
Pin NamePin No.Description of Potential Failure Effect(s)Failure Effect Class
VCCA1Device will not be powered.B
DIR2Pin is floating which can cause excessive current.A
A1 - A83 to 10If configured as output, normal operation. If configured as input, pin is floating which can cause excessive current.A
GND11 to 13Device will not be powered.B
B8 - B114 to 21If configured as output, normal operation. If configured as input, pin is floating which can cause excessive current.A
OE (active low)22Pin is floating which can cause excessive current and cause the outputs to switch between enabled and disabled.B
VCCB23 to 24Device will not be powered.B
Table 4-4 Pin FMA for Device Pins Short-Circuited to Adjacent Pin
Pin NamePin No.Shorted toDescription of Potential Failure Effect(s)Failure Effect Class
VCCA1DIRDirection control will fixed, B --> A direction.B
DIR2A1If DIR is LOW, A1 will be an output and damage is possible. If DIR is HIGH, A1 will be an input and drive the output B1 HIGH.A
A(n)3 to 9A(n+1)If A(n) and A(n+1) are configured as outputs then damage is possible. If configured as inputs, both bits will have the same value alwaysA
A810GNDIf A8 is configured as an output then damage is possible. If configured as input, output B8 will be fixed LOW.A
GND11 to 12GNDNormal Operation.D
GND13B8If B8 is configured as an output then damage is possible. If configured as input, output A8 will be fixed LOW.A
B(n)14 to 20B(n+1)If B(n) and B(n+1) are configured as outputs then damage is possible. If configured as inputs, both bits will have the same value always.A
B121VCCBIf B1 is configured as an output then damage is possible. If configured as an input, no damage, but output A1 will remain HIGH.A
VCCB23 to 24VCCBNormal Operation.D
VCCB24VCCAVCCB short to VCCA, device will be bypassed - may cause system damage, but not device damage.B
Table 4-5 Pin FMA for Device Pins Short-Circuited to supply VCCA
Pin NamePin No.Description of Potential Failure Effect(s)Failure Effect Class
VCCA1Normal Operation.D
DIR2Direction control will fixed, B --> A direction.B
A1 - A83 to 10If configured as an output then damage is possible. If configured as input, no damage, but output will not switch.A
GND11 to 13GND short to VCC, device will be bypassed. This can cause system damage, but not device damage.B
B8 - B114 to 21If configured as an output then damage is possible. If configured as input, damage is possible if VIH/VIL is not met.A
OE (active low)22Outputs will remain disabled.B
VCCB23 to 24VCCB short to VCCA, device will be bypassed. This can cause system damage, but not device damage.B
Table 4-6 Pin FMA for Device Pins Short-Circuited to supply VCCB
Pin NamePin No.Description of Potential Failure Effect(s)Failure Effect Class
VCCA1VCCB short to VCCA, device will be bypassed. This can cause system damage, but not device damage.B
DIR2If VCCA > VCCB, then the direction control will fix A-->B, If VCCA < VCCB, damage is possible if VIH/VIL is not met.A
A1 - A83 to 10If configured as an output then damage is possible. If configured as input, damage is possible if VIH/VIL not met.A
GND11 to 13GND short to VCC, device will be bypassed. This can cause system damage, but not device damage.B
B8 - B114 to 21If configured as an output then damage is possible. If configured as input, no damage, but output will not switch.A
OE (active low)22If VCCA > VCCB, then the outputs will remain disabled, If VCCA < VCCB, damage is possible if VIH/VIL is not met.A
VCCB23 to 24Normal operation.D