See the following resources for further
information about the TI Code Generation Tools:
You can use the following books to
supplement this user's guide:
SLAU132
MSP430 Optimizing C/C++ Compiler User's Guide. Describes the MSP430 C/C++
compiler. This C/C++ compiler accepts ANSI standard C/C++ source code and produces
assembly language source code for the MSP430 devices.
SLAU012
MSP430x3xx Family User's Guide. Describes the MSP430x3xx™ CPU architecture,
instruction set, pipeline, and interrupts for these ultra-low power
microcontrollers.
SLAU049
MSP430x1xx Family User's Guide. Describes the MSP430x1xx™ CPU architecture,
instruction set, pipeline, and interrupts for these ultra-low power
microcontrollers.
SLAU056
MSP430x4xx Family User's Guide. Describes the MSP430x4xx™ CPU architecture,
instruction set, pipeline, and interrupts for these ultra-low power
microcontrollers.
SLAU134
MSP430FE42x ESP30CE1 Peripheral Module User's Guide. Describes common
peripherals available on the MSP430FE42x and ESP430CE1 ultra-low power microcontrollers.
This book includes information on the setup, operation, and registers of the
ESP430CE1.
SLAU144
MSP430x2xx Family User's Guide. Describes the MSP430x2xx™ CPU architecture,
instruction set, pipeline, and interrupts for these ultra-low power
microcontrollers.
SLAU208
MSP430x5xx Family User's Guide. Describes the MSP430x5xx™ CPU architecture,
instruction set, pipeline, and interrupts for these ultra-low power
microcontrollers.
SLAA534
MSP430 Embedded Application Binary Interface. Provides a specification for the
ELF-based Embedded Application Binary Interface (EABI) for the MSP430 family of
processors from Texas Instruments. The EABI defines the low-level interface between
programs, program components, and the execution environment, including the operating
system if one is present.