SLUAAL4 August   2022 BQ21040

 

  1.   Abstract
  2.   Trademarks
  3. 1Introduction
  4. 2How Temperature Sensing Works on the BQ21040
    1. 2.1 With Adapter Present
    2. 2.2 Without Adapter Present
  5. 3Example Application
    1. 3.1 Required Devices
    2. 3.2 Setup
  6. 4Procedure
    1. 4.1 Detecting Adapter Removal
    2. 4.2 Detecting Adapter Insertion
    3. 4.3 Logical Flowchart
  7. 5Summary
  8. 6References

Without Adapter Present

When an adaptor is not present on the BQ21040, the IC is operating in battery only mode. During this mode of operation, there is no 50-uA current being supplied at TS and therefore essentially 0 voltage drop occurs across the NTC thermistor. Without this voltage drop, the method used to obtain temperature measurements with an adapter present as described above cannot be used. Instead, an external MCU will be used to bias 50uA of current across the thermistor. Voltage will then be measured by the MCU in the same manner that the BQ21040 does when an adapter is connected.