SLVAFH4 January 2023 TPS62870 , TPS62870-Q1 , TPS62871 , TPS62871-Q1 , TPS62872 , TPS62872-Q1 , TPS62873 , TPS62873-Q1 , TPS62874-Q1 , TPS62875-Q1 , TPS62876-Q1 , TPS62877-Q1 , TPSM8287A06 , TPSM8287A12 , TPSM8287A15
The output voltage measurements shown in Figure 3-3 show no significant differences of the two converter implementations. The phase shifted synchronization of the dual converter implementation results in a minor improvement at the switching frequency. Since the capacitor bank is the same for both converters and very large in respect to filtering the switching frequency due to load transient requirements the differences in the spectrum are negligible.