SLVAFK5A December 2023 – February 2024 LM5177
Apart from the similar components for power stages, the individual power stage needs some interconnection between each other to make sure proper load sharing and to avoid phase overloads during the parallel operation of the converters. Thus, the Table 2-1 shows the several pins functions which need to be shared between the devices.
Pin function | Pin Name | Comment |
---|---|---|
Softstart | SS/ATRK | Shared soft-start capacitor |
Compensation | COMP | Shared compensations network |
Enable / undervoltage lock out | EN/UVLO | Same voltage level |
Feedback | FB | Shared voltage divider circuit |
Output Voltage | VOUT | Shared output |
Input Voltage | VIN | Shared input |
Bias Voltage | BIAS | Same voltage level |
Moreover, there are some other pins that need to be set as shown in Table 2-2 for accurate parallel operation.
Pin function | Pin Name | Comment |
---|---|---|
RT | RT | Must use the same value for all devices |
External clock | SYNC | To make sure a good load balancing the clock must be phase shifted by 360/n [n = Number of power stages] |
Slope Compensation | SLOPE | Must use the same value for all devices |