SLVK157 October   2023 TPS7H2140-SEP

PRODUCTION DATA  

  1.   1
  2.   TPS7H2140-SEP Neutron Displacement Damage Characterization
  3.   Trademarks
  4. 1Overview
  5. 2Test Procedures
  6. 3Facility
  7. 4Results
    1. 4.1 Data Sheet Electrical Parameters and Associated Tests
  8.   A Appendix: Test Results

Abstract

This report presents the effect of neutron displacement damage (NDD) on the TPS7H2140-SEP device. The results show that all devices were fully functional and within production test limits after having been irradiated up to 1 × 1013 n / cm2 (1-MeV(Si) equivalent.) A sample size of nine units was exposed to radiation testing per MIL-STD-883, Method 1017 for neutron irradiation, and an additional three devices were used as control units and were not irradiated. Electrical testing was performed at Texas Instruments before and after neutron irradiation using the production test program for TPS7H2140-SEP.