SLVU719B May 2012 – November 2021 TPS53819A
Figure 5-2 is a screenshot of the General tab of the Fusion GUI with default configuration where the general configuration parameters can be set. After modifying a parameter the Write to Hardware button must be clicked to apply it. When power cycling all parameters reset to the values stored in flash. To change the values stored in flash, click the Store RAM to Flash button. Figure 5-3 is a screenshot of the All Config tab where all accessible registers are viewed. Figure 5-4 is a screenshot of the Status screen selected on the bottom-left corner. The USB adapter settings are found in the File menu of the Digital Fusion GUI.