SNVA950C April   2020  – March 2024 LM63635-Q1

 

  1.   1
  2. 1Overview
  3. 2Functional Safety Failure In Time (FIT) Rates
    1. 2.1 HTSSOP Package
    2. 2.2 WSON Package
  4. 3Failure Mode Distribution (FMD)
  5. 4Pin Failure Mode Analysis (Pin FMA)
    1. 4.1 HTSSOP Package
    2. 4.2 WSON Package
  6. 5Revision History

HTSSOP Package

Figure 4-1 shows the LM63635-Q1 pin diagram for the HTSSOP package. For a detailed description of the device pins, please refer to the Pin Configuration and Functions section in the LM63635 data sheet.

GUID-11C76DD3-5C08-47FA-9EE3-5181BD629D0A-low.gifFigure 4-1 Pin Diagram for HTSSOP
Table 4-2 Pin FMA for Device Pins Short-Circuited to Ground
Pin NamePin No.Description of Potential Failure Effect(s)Failure Effect Class
SW1,2Damage to internal power FET(s) and other internal circuitsA
BOOT3Damage to internal circuitsA
VCC4Fault mode will shut device offB
RT5Depends on exact application configuration. For application circuit as shown in the Example Application Circuit in the device data sheet, no effect will be produced. If an RT resistor is used the frequency will be set to 2.1MHz. If a 0Ω jumper is used to connect the RT input to VCC, then the VCC output will be pulled to ground; see short to ground on pin 4.B
VSEL6Depends on exact application configuration. For an application circuit as shown in the Example Application Circuit in the device data sheet, VCC will be shorted to ground; see short to ground on pin 4. If a VSEL resistor is used, or if the VSEL input is pulled to ground with a 0Ω jumper, then the output voltage will be set to 3.3V, before power-up. No effect after power-up.B
SYNC/MODE7Depends on exact application configuration. For an application circuit as shown in the Example Application Circuit in the device data sheet, no effect will be produced. If a 0Ω jumper is used to connect the SYNC/MODE input to VCC, then the VCC output will be pulled to ground; see short to ground on pin 4.B
RESET8RESET functionality will be lost.B
FB9The regulator will operate at maximum duty cycle. Output voltage will rise to nearly the input voltage (VIN) level. Possible damage to customer load and output stage components may occur. No effect on device.B
AGND10No effectD
EN11Loss of ENABLE functionality Device will remain in shut-down mode.B
VIN12,13Device will not operate. No output voltage will be generated. Output capacitors will discharge through input short. Large reverse current may damage device.A
N/C14No effectD
PGND15,16No effectD
Table 4-3 Pin FMA for Device Pins Open-Circuited
Pin NamePin No.Description of Potential Failure Effect(s)Failure Effect Class
SW1,2With both pins open, there can be a loss of output voltage. With one pin open, there can be some loss of device performance.B
BOOT3Loss of output voltage regulation; low or no output voltage.B
VCC4VCC LDO will be unstable. Loss of output voltage regulation and possible damage to internal circuits.A
RT5Device switching frequency will drop to zero or become erratic. Loss of output voltage.B
VSEL6Device will enter ADJ mode when EN or VIN is cycled. Incorrect output voltage if fixed VOUT mode was intended. No effect after power-up.C
SYNC/MODE7Internal pull-down will place device in AUTO mode.B
RESET8RESET functionality will be lost.B
FB9Loss of output voltage regulation. Output voltage may rise or fall outside of intended regulation window.B
AGND10Loss of output voltage regulation. Possible damage to internal circuits.A
EN11Loss of ENABLE functionality. Erratic operation; probable loss of regulation.B
VIN12,13With both pins open: loss of output voltage. With one pin open: possible device damage.A
N/C14No effectD
PGND15,16With either one or both pins open, possible device damage.A
Table 4-4 Pin FMA for Device Pins Short-Circuited to Adjacent Pin
Pin NamePin No.Shorted toDescription of Potential Failure Effect(s)Failure Effect Class
SW1SWNo effectD
SW2BOOTLoss of output regulation, possible damage to internal circuitsA
BOOT3VCCLoss of output regulation, possible damage to internal circuitsA
VCC4RTDepends on exact application configuration. For an application circuit as shown in the Example Application Circuit in the device data sheet, VCC will be shorted to ground; see short to ground on pin 4. For all other configurations, the effect will either be no change or erratic switching frequency with possible damage to device internal circuits.A
RT5VSELDepends on exact application configuration. For an application circuit as shown in the Example Application Circuit in the device data sheet, VCC will be shorted to ground; see short to ground on pin 4. For all other configurations, the effect will either be no change or erratic output voltage and switching frequency with possible damage to device internal circuits.A
VSEL6SYNC/MODEDepends on exact application configuration. For an application circuit as shown in the Example Application Circuit in the device data sheet, VCC will be shorted to ground; see short to ground on pin 4. For all other configurations, the effect will either be no change or erratic operation and switching frequency with possible damage to device internal circuits.A
SYNC/MODE7RESETDepends on exact application configuration. For an application circuit as shown in the Example Application Circuit in the device data sheet, RESET will be shorted to ground; see short to ground on pin 8. For all other configurations, the effect will either be no change or erratic operation and loss of RESET and/or SYNC/MODE functionality with possible damage to device internal circuits.A
FB9AGNDSee see short to ground on pin 9B
AGND10ENSee see short to ground on pin 11B
EN11VINSee see short to VIN on pin 11B
VIN12,13N/CNo effectD
N/C14PGNDNo effectD
Table 4-5 Pin FMA for Device Pins Short-Circuited to VIN
Pin NamePin No.Description of Potential Failure Effect(s)Failure Effect Class
SW1,2Damage to internal power FET(s) and other internal circuitsA
BOOT3Damage to internal circuitsA
VCC4Damage to internal circuits for VIN >5.5VA
RT5Depends on exact application configuration. For an application circuit as shown in the Example Application Circuit in the device data sheet, no damage will occur. For all other configurations, damage to internal circuits will occur for VIN >5.5V.A
VSEL6Damage to internal circuits for VIN >5.5VA
SYNC/MODE7Depends on exact application configuration. For an application circuit as shown in the Example Application Circuit in the device data sheet, no damage will occur. For all other configurations, damage to internal circuits will occur for VIN >5.5V.A
RESET8Damage to internal circuits.A
FB9Depends on exact application configuration. For an application circuit as shown in the Example Application Circuit in the device data sheet, damage to internal circuits will occur for VIN >16V. For operation in the ADJ mode, damage to internal circuits will occur for VIN >5.5V.A
AGND10Possible damage to internal circuits or packageA
EN11No damage to device. Loss of ENABLE functionality.B
VIN12,13No effect.D
N/C14No effect.D
PGND15,16Possible damage to internal circuits or packageA