SNVAA61 February 2023 LM5168 , LM5168-Q1 , LM5169 , LM5169-Q1
A new bypass capacitance, from VIN to -VOUT is used to help with load transients. The value for the bypass capacitance, CIO, can be chosen using input capacitance recommendations from the buck datasheet, but it is important to note that the voltage across the capacitors will be VIN + |-VOUT|. The capacitors used should be appropriately sized for the voltage difference between VIN and -VOUT. When the input supply is turned on, the bypass capacitance may cause the output to shortly swing positive before becoming negative. If the desired load is sensitive to a positive swing, then an optional Schottky diode can be placed across the output to clamp the voltage.