SPRACT6A october 2020 – march 2023 TMS320F2800132 , TMS320F2800132 , TMS320F2800133 , TMS320F2800133 , TMS320F2800135 , TMS320F2800135 , TMS320F2800137 , TMS320F2800137 , TMS320F2800152-Q1 , TMS320F2800152-Q1 , TMS320F2800153-Q1 , TMS320F2800153-Q1 , TMS320F2800154-Q1 , TMS320F2800154-Q1 , TMS320F2800155 , TMS320F2800155 , TMS320F2800155-Q1 , TMS320F2800155-Q1 , TMS320F2800156-Q1 , TMS320F2800156-Q1 , TMS320F2800157 , TMS320F2800157 , TMS320F2800157-Q1 , TMS320F2800157-Q1 , TMS320F280021 , TMS320F280021 , TMS320F280021-Q1 , TMS320F280021-Q1 , TMS320F280023 , TMS320F280023 , TMS320F280023-Q1 , TMS320F280023-Q1 , TMS320F280023C , TMS320F280023C , TMS320F280025 , TMS320F280025 , TMS320F280025-Q1 , TMS320F280025-Q1 , TMS320F280025C , TMS320F280025C , TMS320F280025C-Q1 , TMS320F280025C-Q1 , TMS320F280033 , TMS320F280033 , TMS320F280034 , TMS320F280034 , TMS320F280034-Q1 , TMS320F280034-Q1 , TMS320F280036-Q1 , TMS320F280036-Q1 , TMS320F280036C-Q1 , TMS320F280036C-Q1 , TMS320F280037 , TMS320F280037 , TMS320F280037-Q1 , TMS320F280037-Q1 , TMS320F280037C , TMS320F280037C , TMS320F280037C-Q1 , TMS320F280037C-Q1 , TMS320F280038-Q1 , TMS320F280038-Q1 , TMS320F280038C-Q1 , TMS320F280038C-Q1 , TMS320F280039 , TMS320F280039 , TMS320F280039-Q1 , TMS320F280039-Q1 , TMS320F280039C , TMS320F280039C , TMS320F280039C-Q1 , TMS320F280039C-Q1 , TMS320F280040-Q1 , TMS320F280040-Q1 , TMS320F280040C-Q1 , TMS320F280040C-Q1 , TMS320F280041 , TMS320F280041 , TMS320F280041-Q1 , TMS320F280041-Q1 , TMS320F280041C , TMS320F280041C , TMS320F280041C-Q1 , TMS320F280041C-Q1 , TMS320F280045 , TMS320F280045 , TMS320F280048-Q1 , TMS320F280048-Q1 , TMS320F280048C-Q1 , TMS320F280048C-Q1 , TMS320F280049 , TMS320F280049 , TMS320F280049-Q1 , TMS320F280049-Q1 , TMS320F280049C , TMS320F280049C , TMS320F280049C-Q1 , TMS320F280049C-Q1 , TMS320F28075 , TMS320F28075 , TMS320F28075-Q1 , TMS320F28075-Q1 , TMS320F28076 , TMS320F28076 , TMS320F28374D , TMS320F28374D , TMS320F28374S , TMS320F28374S , TMS320F28375D , TMS320F28375D , TMS320F28375S , TMS320F28375S , TMS320F28375S-Q1 , TMS320F28375S-Q1 , TMS320F28376D , TMS320F28376D , TMS320F28376S , TMS320F28376S , TMS320F28377D , TMS320F28377D , TMS320F28377D-EP , TMS320F28377D-EP , TMS320F28377D-Q1 , TMS320F28377D-Q1 , TMS320F28377S , TMS320F28377S , TMS320F28377S-Q1 , TMS320F28377S-Q1 , TMS320F28378D , TMS320F28378D , TMS320F28378S , TMS320F28378S , TMS320F28379D , TMS320F28379D , TMS320F28379D-Q1 , TMS320F28379D-Q1 , TMS320F28379S , TMS320F28379S , TMS320F28384D , TMS320F28384D , TMS320F28384D-Q1 , TMS320F28384D-Q1 , TMS320F28384S , TMS320F28384S , TMS320F28384S-Q1 , TMS320F28384S-Q1 , TMS320F28386D , TMS320F28386D , TMS320F28386D-Q1 , TMS320F28386D-Q1 , TMS320F28386S , TMS320F28386S , TMS320F28386S-Q1 , TMS320F28386S-Q1 , TMS320F28388D , TMS320F28388D , TMS320F28388S , TMS320F28388S , TMS320F28P650DH , TMS320F28P650DH , TMS320F28P650DK , TMS320F28P650DK , TMS320F28P650SH , TMS320F28P650SH , TMS320F28P650SK , TMS320F28P650SK , TMS320F28P659DH-Q1 , TMS320F28P659DH-Q1 , TMS320F28P659DK-Q1 , TMS320F28P659DK-Q1 , TMS320F28P659SH-Q1 , TMS320F28P659SH-Q1
Table 3-3 shows the completed worksheet for the F280049 with OPA2350 example.
Symbol | Description | Value | Comments |
---|---|---|---|
Vfs | Full scale voltage range | 3.0 V | In external reference mode,
this is the voltage supplied to the VREFHI pin (usually 3.0 V or 2.5 V)
In internal reference mode, this is the effective input range based on the selected reference mode (usually 3.3 V or 2.5 V) |
N | Target settling resolution (bits) | 12 bits | Usually the same as the
resolution of the ADC Lower resolution can be targeted to relax the input design requirements |
Verrmax | Maximum error target | 366 uV | Vfs /
2N+1 Obtain using Analog Engineer's Calculator: ADC SAR Drive |
tsh | S+H time | 100 ns | Enter target S+H time if
known Longer S+H times will result in less stringent BW requirements for the driving op-amp. Can be solved for given a pre-determined op-amp selection or a pre-determined RS and CS |
Ron | ADC switch resistance | 500 Ω | Provided in the data manual
table "Input Model Parameters" TI precision labs training refers to this as "Rsh" |
Ch | ADC S+H capacitance | 12.5 pF | Provided in the data manual
table "Input Model Parameters" TI precision labs training refers to this as "Csh" |
Cp | ADC pin parasitic capacitance | 12.7 pF | Provided in the data manual table "Per-Channel Parasitic Capacitance" |
CS (range) | Range of source capacitance | 240 pF (120pF to 360pF) |
Obtain using Analog
Engineer's Calculator: ADC SAR Drive. TI precision labs training refers to this as "Cfilt" |
RS (range) | Range of source resistance | 17 to 138 Ω | Obtain using Analog
Engineer's Calculator: ADC SAR Drive. TI precision labs training refers to this as "Rfilt" |
BWOPA | ADC driver op-amp minimum bandwidth | 37 MHz | Obtain using Analog Engineer's Calculator: ADC SAR Drive. |
Op-amp | Selected Op-amp part number | OPA2350 | Record selected op-amp here |
Voa_ss | Steady state op-amp output voltage | 3.000014 V | Generated from DC nodal
analysis of the Voa node Copy to Voa_ss before proceeding with other simulations |
CS (final) | Final source capacitance | 240 pF | Final selected CS
from simulation. TI precision labs training refers to this as "Cfilt" |
RS (final) | Final source resistance | 27 Ω | Final selected RS
from simulation. TI precision labs training refers to this as "Rfilt" |
BWRsCs | Filter bandwidth from CS and RS | 2.5 MHz | 1 /
(2π·CS·RS ) Note: For proper settling,
the filter bandwidth will be necessarily higher than the ½ the
sampling frequency, thus the combination of CS and
RS generally will not function as an anti-aliasing
filter. |
Verr | Actual settling error | 17 μV | Ensure Verr <
Verrmax Othwerwise, additional iteration on selection of CS , RS , or the driving amplifier is needed |