SPRACW9A June   2021  – March 2023 TMS320F2800132 , TMS320F2800132 , TMS320F2800133 , TMS320F2800133 , TMS320F2800135 , TMS320F2800135 , TMS320F2800137 , TMS320F2800137 , TMS320F2800152-Q1 , TMS320F2800152-Q1 , TMS320F2800153-Q1 , TMS320F2800153-Q1 , TMS320F2800154-Q1 , TMS320F2800154-Q1 , TMS320F2800155 , TMS320F2800155 , TMS320F2800155-Q1 , TMS320F2800155-Q1 , TMS320F2800156-Q1 , TMS320F2800156-Q1 , TMS320F2800157 , TMS320F2800157 , TMS320F2800157-Q1 , TMS320F2800157-Q1 , TMS320F280021 , TMS320F280021 , TMS320F280021-Q1 , TMS320F280021-Q1 , TMS320F280023 , TMS320F280023 , TMS320F280023-Q1 , TMS320F280023-Q1 , TMS320F280023C , TMS320F280023C , TMS320F280025 , TMS320F280025 , TMS320F280025-Q1 , TMS320F280025-Q1 , TMS320F280025C , TMS320F280025C , TMS320F280025C-Q1 , TMS320F280025C-Q1 , TMS320F280033 , TMS320F280033 , TMS320F280034 , TMS320F280034 , TMS320F280034-Q1 , TMS320F280034-Q1 , TMS320F280036-Q1 , TMS320F280036-Q1 , TMS320F280036C-Q1 , TMS320F280036C-Q1 , TMS320F280037 , TMS320F280037 , TMS320F280037-Q1 , TMS320F280037-Q1 , TMS320F280037C , TMS320F280037C , TMS320F280037C-Q1 , TMS320F280037C-Q1 , TMS320F280038-Q1 , TMS320F280038-Q1 , TMS320F280038C-Q1 , TMS320F280038C-Q1 , TMS320F280039 , TMS320F280039 , TMS320F280039-Q1 , TMS320F280039-Q1 , TMS320F280039C , TMS320F280039C , TMS320F280039C-Q1 , TMS320F280039C-Q1 , TMS320F280040-Q1 , TMS320F280040-Q1 , TMS320F280040C-Q1 , TMS320F280040C-Q1 , TMS320F280041 , TMS320F280041 , TMS320F280041-Q1 , TMS320F280041-Q1 , TMS320F280041C , TMS320F280041C , TMS320F280041C-Q1 , TMS320F280041C-Q1 , TMS320F280045 , TMS320F280045 , TMS320F280048-Q1 , TMS320F280048-Q1 , TMS320F280048C-Q1 , TMS320F280048C-Q1 , TMS320F280049 , TMS320F280049 , TMS320F280049-Q1 , TMS320F280049-Q1 , TMS320F280049C , TMS320F280049C , TMS320F280049C-Q1 , TMS320F280049C-Q1 , TMS320F28075 , TMS320F28075 , TMS320F28075-Q1 , TMS320F28075-Q1 , TMS320F28076 , TMS320F28076 , TMS320F28374D , TMS320F28374D , TMS320F28374S , TMS320F28374S , TMS320F28375D , TMS320F28375D , TMS320F28375S , TMS320F28375S , TMS320F28375S-Q1 , TMS320F28375S-Q1 , TMS320F28376D , TMS320F28376D , TMS320F28376S , TMS320F28376S , TMS320F28377D , TMS320F28377D , TMS320F28377D-EP , TMS320F28377D-EP , TMS320F28377D-Q1 , TMS320F28377D-Q1 , TMS320F28377S , TMS320F28377S , TMS320F28377S-Q1 , TMS320F28377S-Q1 , TMS320F28378D , TMS320F28378D , TMS320F28378S , TMS320F28378S , TMS320F28379D , TMS320F28379D , TMS320F28379D-Q1 , TMS320F28379D-Q1 , TMS320F28379S , TMS320F28379S , TMS320F28384D , TMS320F28384D , TMS320F28384D-Q1 , TMS320F28384D-Q1 , TMS320F28384S , TMS320F28384S , TMS320F28384S-Q1 , TMS320F28384S-Q1 , TMS320F28386D , TMS320F28386D , TMS320F28386D-Q1 , TMS320F28386D-Q1 , TMS320F28386S , TMS320F28386S , TMS320F28386S-Q1 , TMS320F28386S-Q1 , TMS320F28388D , TMS320F28388D , TMS320F28388S , TMS320F28388S , TMS320F28P650DH , TMS320F28P650DH , TMS320F28P650DK , TMS320F28P650DK , TMS320F28P650SH , TMS320F28P650SH , TMS320F28P650SK , TMS320F28P650SK , TMS320F28P659DH-Q1 , TMS320F28P659DH-Q1 , TMS320F28P659DK-Q1 , TMS320F28P659DK-Q1 , TMS320F28P659SH-Q1 , TMS320F28P659SH-Q1

 

  1.   Abstract
  2.   Trademarks
  3. 1Introduction
    1. 1.1 Memory Cross-Talk Challenges
    2. 1.2 Resources for Signal Conditioning Circuit Design
      1. 1.2.1 TI Precision Labs - SAR ADC Input Driver Design Series
      2. 1.2.2 Analog Engineer's Calculator
      3. 1.2.3 Related Application Reports
      4. 1.2.4 TINA-TI SPICE-Based Analog Simulation Program
      5. 1.2.5 PSPICE for TI
      6. 1.2.6 ADC Input Circuit Evaluation for C2000 MCUs
      7. 1.2.7 Charge-Sharing Driving Circuits for C2000 ADCs
  4. 2Review of ADC Input Settling
    1. 2.1 Mechanism of ADC Input Settling
    2. 2.2 Symptoms of Inadequate Settling
      1. 2.2.1 Distortion
      2. 2.2.2 Memory Cross-Talk
      3. 2.2.3 Accuracy
    3. 2.3 C2000 ADC Architecture
  5. 3Problem Statement
    1. 3.1 Example System
    2. 3.2 S+H Settling Analysis
    3. 3.3 Charge-Sharing Analysis
    4. 3.4 Problem Summary
  6. 4Dedicated ADC Sampling
    1. 4.1 Dedicated ADC Concept
    2. 4.2 Settling Mechanism for Dedicated ADC
    3. 4.3 Design Flow for Dedicated ADC
    4. 4.4 Simulating Settling Performance for a Dedicated ADC Circuit
  7. 5Pre-Sampling VREFLO
    1. 5.1 VREFLO Sampling Concept
    2. 5.2 Properties of VREFLO Sampling Method Error
    3. 5.3 Gain Error Compensation
      1. 5.3.1 Methods for Determining Compensation Coefficients
    4. 5.4 VREFLO Sampling Design Flow
    5. 5.5 Discussion of VREFLO Sampling Sequences
  8. 6Summary
  9. 7References
  10. 8Revision History

VREFLO Sampling Concept

In Section 3.1, an example system that sampled four voltages was presented. One of these voltages, V2, was specified to have poor settling performance (due to excessively high source impedance from using a voltage divider to drive the ADC input directly). Figure 5-1 shows one possible re-organization of the sampling scheme where a sample of VREFLO (zero-scale) has been added before the channel in question. The result of this is to replace memory cross-talk from voltage V1 (which is an independent signal that could take on any voltage at any time) with memory cross-talk from VREFLO (that reliably produces cross-talk that pulls V2 towards exactly 0 V).

GUID-AE1C93A1-0366-4512-B8AE-C9C960F8B538-low.png Figure 5-1 Timings for VREFLO Sampling Method

Unlike the single-ADC method, it is possible to apply the pre-sampling VREFLO methodology to multiple signals on the same ADC. This method is only limited by the number spare start-of-conversion (SOC) structures available in the ADC wrapper to sequence the extra conversions (no external pins are needed) and the amount of additional latency spent processing the VREFLO samples that the application can tolerate. Later sections will also show that a light post-processing of the ADC results is also desirable. Performing this operation will add some additional latency that will also need to be absorbed by the application.