SPRUIV4C May 2020 – December 2023
In some instances, functional calls inhibit optimization. For instance, a loop containing a function call will not be software pipelined if the compiler is not able to inline the called function. In order to enable optimizations such as software pipelining, it may be necessary to define the called function in one of these ways:
The compiler performs some amount of automatic inlining at the --opt_level=3 and --opt_level=4 optimization levels.