SWRA571B August 2017 – August 2020 CC1310 , CC1310 , CC1312PSIP , CC1312PSIP , CC1312R , CC1312R , CC1314R10 , CC1314R10 , CC1350 , CC1350 , CC1352P , CC1352P , CC1352P7 , CC1352P7 , CC1352R , CC1352R
When using the IQ Dump patch in RX the data rate is limited upwards to 12.5 kbps for CC13x0 and 25 kbps for CC13x2. In TX, the patch can be used within the same operating limits as the genfsk/prop PHY. The 50-kbps settings from SmartRF™ Studio [1] should be used as a starting point. The associated zip file contains a smartrf_settings.c file (for CC1310) that has the complete override list and API settings to be used with the patch.