SWRA601K April 2019 – November 2023 CC1350 , CC1352P , CC1352P7 , CC1352R , CC2340R5 , CC2540 , CC2540T , CC2541 , CC2541-Q1 , CC2640 , CC2640R2F , CC2640R2F-Q1 , CC2642R , CC2642R-Q1 , CC2650 , CC2650MODA , CC2652P , CC2652R , CC2652R7 , CC2652RB , CC2652RSIP
Errata are corrections to Bluetooth specifications provided after the specification in question is adopted. If the erratum is adopted after Texas Instruments has produced the QDL and the corresponding QDID, extra documentation will be required to go through the qualification process. The list of the specification errata is available on the Bluetooth website [14].