SWRA640H December 2018 – May 2024 CC1310 , CC1312R , CC1314R10 , CC1350 , CC1352P , CC1352R , CC1354P10 , CC1354R10 , CC2620 , CC2630 , CC2640 , CC2640R2F , CC2640R2F-Q1 , CC2642R , CC2642R-Q1 , CC2650 , CC2652P , CC2652R , CC2652R7 , CC2652RB , CC2652RSIP , CC2674P10 , CC2674R10
A balun is a network that transforms from a balanced (differential) to an unbalanced (single-ended) signal. The design is a lumped, lattice-type LC that has a ±90° phase shift implemented by using a low-pass filter and a high-pass filter. It is important to keep the balun as symmetrical as possible. If only one of the RF pins is used for RF output/input, no balun is required. In this case a filter is required between the chip and the antenna. For more details, see Section 2.3.