SWRU473A February 2017 – August 2018 CC3120MOD , CC3220MOD , CC3220MODA , CC3220R , CC3220S , CC3220SF
Using the SimpleLink Wi-Fi Starter Pro application, users can start AP provisioning or SmartConfig provisioning for a fast CC3220 connection. During this procedure, the AP credentials are decoded by the CC3220, and a profile is stored on the serial flash for future connections.
By default, the OOB application starts in provisioning mode. Provisioning mode is reflected by a flashing red LED (D7) once every 2 seconds. The terminal can also be used for extra debug messages. The Waiting to be Provisioned message appears when the device is ready to be provisioned.
The provisioning procedure for SmartConfig is described as follows.
Additional LAN and OTA tabs are applicable only to the OOB and automatically open after provisioning is successfully completed. If these tabs do not show up, navigate to the Devices tab and select the device by pressing and holding it.