SWRU602 September 2023 CC3300 , CC3301
The following kernel configuration is a prerequisite for correct Calibrator Tool operation:
root@am335x-evm:/usr/share/cc33xx# zcat /proc/config.gz | grep NL80211_TESTMODE
Where the output is:
CONFIG_NL80211_TESTMODE=y
If the configuration is not enabled in the driver, you need to recompile kernel and kernel modules and install them to the device. For more informaiton on how to enable this flag and integrate the changes, see the CC33xx Linux Getting Started User's Guide in the CC33xx Linux Software Package.
ifconfig wlan0 down
to disable the wlan0 interface. Verify the wlan0 interface is disabled by running the ifconfig
command again. There should not be any mention of wlan0
on the output of ifconfig
.