Setting up
communication via a USB interface for the controller board is similar to the set up
for SPI communication via the Cheetahâ„¢ host adapter.
- Start the DLPC230-Q1 Control Program Lite.
- With the DLPC231 controller board off, short pins 2-3 together on jumpers
J10, J11, J12, and J13 of the controller board using a jumper
- On the connection page, set the DLPC230-Q1 Host to SPI and
select the
Cypress
option from the drop down
menu.
- The
"Connection" Settings can be left the same way they were previously for SPI
communication.
- Click the
Connect
button. The green circle next to the Connect button
then lights up to indicate that connection was successful to
USB.