SBAA447 September   2021 AMC1302-Q1

 

  1.   Trademarks
  2. 1Overview
  3. 2Functional Safety Failure In Time (FIT) Rates
  4. 3Failure Mode Distribution (FMD)
  5. 4Pin Failure Mode Analysis (Pin FMA)

Pin Failure Mode Analysis (Pin FMA)

This section provides a failure mode analysis (FMA) for the pins of the AMC1302-Q1. The failure modes covered in this document include the typical pin-by-pin failure scenarios:

  • Pin short-circuited to ground (see Table 4-2)
  • Pin open-circuited (see Table 4-3)
  • Pin short-circuited to an adjacent pin (see Table 4-4)
  • Pin short-circuited to supply (see Table 4-5)

Table 4-2 through Table 4-5 also indicate how these pin conditions can affect the device as per the failure effects classification in Table 4-1.

Table 4-1 TI Classification of Failure Effects
Class Failure Effects
A Potential device damage that affects functionality
B No device damage, but loss of functionality
C No device damage, but performance degradation
D No device damage, no impact to functionality or performance

Figure 4-1 shows the AMC1302-Q1 pin diagram. For a detailed description of the device pins see the Pin Configuration and Functions section in the AMC1302-Q1 data sheet.

Figure 4-1 Pin Diagram

Following are the assumptions of use and the device configuration assumed for the pin FMA in this section:

  • Differential RC filter between INP and INN.
    The series resistors are sized to limit the input currents into INP and INN to <10 mA in all circumstances (for example, if the device is unpowered and the input signal is applied).
  • INN is connected to GND1 through the filter resistor.
  • For pins on high side:
    Short-circuited to ground means short to GND1.
    Short-circuited to supply means short to VDD1.
  • For pins on low side:
    Short-circuited to ground means short to GND2.
    Short-circuited to supply means short to VDD2.

Table 4-2 Pin FMA for Device Pins Short-Circuited to Ground
Pin Name Pin No. Description of Potential Failure Effect(s) Failure Effect Class
VDD1 1 Device high side unpowered. Fail-safe output (see data sheet for more details). B
INP 2 INP stuck low (GND1). Differential output (VOUTP – VOUTN) = –VINN x 41 with common-mode voltage approximately 1.44 V. B
INN 3 INN stuck low (GND1). Differential output (VOUTP – VOUTN) = VINP x 41 with common-mode voltage approximately 1.44 V. D
GND1 4 No effect. Normal operation. D
GND2 5 No effect. Normal operation. D
OUTN 6 OUTN stuck low (GND2). Excess current consumption from VDD2 source. Device damage plausible if condition is present for extended period of time. A
OUTP 7 OUTP stuck low (GND2). Excess current consumption from VDD2. Device damage plausible if condition is present for extended period of time. A
VDD2 8 Device low side unpowered. OUTP and OUTN pins are driven to GND2. B
Table 4-3 Pin FMA for Device Pins Open-Circuited
Pin Name Pin No. Description of Potential Failure Effect(s) Failure Effect Class
VDD1 1 Device high side unpowered. Fail-safe output (see data sheet for more details). B
INP 2 Differential output (VOUTP – VOUTN) undetermined, but with tendency to output +FS. B
INN 3 Differential output (VOUTP – VOUTN) undetermined. B
GND1 4 Device high side unpowered. Fail-safe output (see data sheet for more details). B
GND2 5 Device behavior undetermined. VOUTN and VOUTP undetermined. B
OUTN 6 Differential output (VOUTP – VOUTN) undetermined. B
OUTP 7 Differential output (VOUTP – VOUTN) undetermined. B
VDD2 8 Device low side unpowered. VOUTN and VOUTP undetermined. B
Table 4-4 Pin FMA for Device Pins Short-Circuited to Adjacent Pin
Pin Name Pin No. Shorted to Description of Potential Failure Effect(s) Failure Effect Class
VDD1 1 INP INP stuck high (VDD1). In case VCM < VCMov, differential output (VOUTP – VOUTN) = +FS. In case VCM ≥ VCMov, fail-safe output (see data sheet for more details). B
INP 2 INN Differential input shorted. Differential output (VOUTP – VOUTN) = 0 V B
INN 3 GND1 INN stuck low (GND1). Differential output (VOUTP – VOUTN) = VINP x 41 with common-mode voltage approximately 1.44 V. D
GND1 4 GND2 Not considered. Corner pin. D
GND2 5 OUTN OUTN stuck low (GND2). Excess current consumption from VDD2 source. Device damage plausible if condition is present for extended period of time. A
OUTN 6 OUTP Differential output (VOUTP – VOUTN) = 0 V with common-mode voltage approximately 1.44 V. Excess current consumption from VDD2 source. Device damage plausible if condition is present for extended period of time. A
OUTP 7 VDD2 OUTP stuck high (VDD2). Excess current consumption from VDD2 source. Device damage plausible if condition is present for extended period of time. A
VDD2 8 VDD1 Not considered. Corner pin. D
Table 4-5 Pin FMA for Device Pins Short-Circuited to Supply
Pin Name Pin No. Description of Potential Failure Effect(s) Failure Effect Class
VDD1 1 No effect. Normal operation. D
INP 2 INP stuck high (VDD1). In case VCM < VCMov, differential output (VOUTP – VOUTN) = +FS. In case VCM ≥ VCMov, fail-safe output (see data sheet for more details). B
INN 3 INN stuck high (VDD1). In case VCM < VCMov, differential output (VOUTP – VOUTN) incorrect. In case VCM ≥ VCMov, fail-safe output (see data sheet for more details). B
GND1 4 Device high side unpowered. Fail-safe output (see data sheet for more details). B
GND2 5 Device low side unpowered. OUTP and OUTN pins are driven to GND2. B
OUTN 6 OUTN stuck high (VDD2). Excess current consumption from VDD2 source. Device damage plausible if condition is present for extended period of time. A
OUTP 7 OUTP stuck high (VDD2). Excess current consumption from VDD2 source. Device damage plausible if condition is present for extended period of time. A
VDD2 8 No effect. Normal operation. D