SBAU428 September   2023 AFE7769D

 

  1.   Abstract
  2.   2
  3.   Trademarks
  4. 1Introduction
  5. 2Hardware Setup
  6. 3Software Setup
  7. 4Bring-Up Steps
  8. 5TX to FB Loopback With DDR Example
  9.   A Setting Ethernet Port IP Address

Setting Ethernet Port IP Address

  1. Go to "Ethernet" under settings and double click on the "Ethernet" port connected to the Agilex eSOM7.
    GUID-20230804-SS0I-07PS-SCMV-T7VJNX8RNP9W-low.png Figure A-1 Ethernet Settings
  2. Under IP settings, click the “Edit” button and select “Manual” on the drop down to set the IP address manually as shown in Figure 6-2. After changing the “IP address”, “Subnet prefix length”, and “Gateway” fields, click “Save”.
    GUID-20230804-SS0I-1BJ6-QFCP-KD0Z2T6Q8C4R-low.png Figure A-2 Manually Setting IP Address
  3. After that, open the Control Panel and navigate to “Control Panel\Network and Internet\Network and Sharing Center”. Then, click on the connection for the Agilex eSOM7 as shown in Figure 6-3.
    GUID-20230804-SS0I-XRP8-NLCS-BJFS51CCRWVM-low.png Figure A-3 Opening the Network in Control Panel
  4. A window as shown in Figure 6-4 will appear. Click the “Properties” button.
    GUID-20230804-SS0I-KDSG-XB5T-HMVCWJRVMCS1-low.png Figure A-4 Opening the Properties Tab for the Ethernet Connection
  5. After that a window as shown in Figure 6-5 will open. Double click the “Internet Protocol Version 4 (TCP/IPv4)” option to open its "Properties" tab.
    GUID-20230804-SS0I-CJJ3-7ZKP-6XMNFVV5HH1F-low.png Figure A-5 Opening the IPv4 Properties
  6. In the window that opens select the “Use the following IP address” option and fill out the fields as shown in Figure 6-6. After filling out the fields click ok and the address will be set.
    GUID-20230804-SS0I-7PLG-WXGM-1QHCNWFQKDVB-low.png Figure A-6 Setting the IP Address Manually