SLLU149E June 2011 – February 2016 TUSB7320 , TUSB7340
The TUSB73x0 has an x1 PCI Express interface that runs at 5-Gb/s and is fully compliant to the PCI Express Base Specification, Revision 2.0.
The TUSB73x0 TX and RX terminals attach to the upstream PCI Express device over a 5-Gb/s high-speed differential transmit and receive PCI Express x1 Link. The connection details are provided in the following table.
It is permissible to swap the plus and minus on either or both of the PCIe differential pairs. This may be necessary to prevent the differential traces from crossing over one another. However it is not permissible to swap the transmitter differential pair with the receive differential pair.
In order to minimize cross-talk on the PCIe differential signal pair, it is recommended that the spacing between the TX and RX signal pairs for each interface be five times the width of the trace (5W rule). For instance, if the PCIe TX differential pair trace width is 5 mils, then there should be 25 mils of space between the TX and RX differential pairs.
If this 5W rule cannot be implemented, then the space between the TX and RX differential pairs should be maximized as much as possible and ground-fill should be placed between the two. In this case, it is better to route each differential pair on opposite sides of the board with a ground plane between them.
TUSB73x0 Terminal Name | Upstream PCIe Device
Terminal Name |
Description |
---|---|---|
TXP | RXP | TUSB73x0 transmit positive differential terminal connects to the upstream device receive positive differential terminal. |
TXP | RXN | TUSB73x0 transmit negative differential terminal connects to the upstream device receive negative differential terminal. |
RXP | TXP | TUSB73x0 receive positive differential terminal connects to the upstream device transmit positive differential terminal. |
RXN | TXP | TUSB73x0 receive negative differential terminal connects to the upstream device transmit negative differential terminal. |
The TUSB73x0 TXP and TXN terminals comprise a low-voltage, 100-Ω differential signal pair. The RXP and RXN terminals for the TUSB73x0 receive a low-voltage, 100-Ω differential signal pair. The TUSB73x0 has integrated 50-Ω termination resistors to VSS on both the RXP and RXN terminals eliminating the need for external components.
The TX lane of the differential signal pair must be ac-coupled. The recommended value for the series capacitor is 0.1 μF. To minimize stray capacitance associated with the series capacitor circuit board solder pads, 0402 sized capacitors are recommended.
When routing a 5-Gb/s low-voltage, 100-Ω differential signal pair, the following circuit board design guidelines must be considered: