SLUAAM4 December 2023 BQ76905 , BQ76907
BQStudio has an Auto Refresh on the Dashboard that periodically reads the registers of the device to refresh the measurements displayed. When using the Command Sequence module, the recommendation is to disable Auto Refresh by clicking on the green banner. The banner turns red to indicate Auto Refresh is disabled (see Figure 1-6).