SLUUCO9A April 2023 – November 2023 BQ28Z620
This command returns the CellVoltages, PackVoltage, BatVoltage, CellCurrents, CellPowers, Power, and AveragePower on MACData().
Status | Condition | Action |
---|---|---|
Activate | 0x0071 to MACSubcmd() | Outputs 32 bytes of data on MACData() in the following format: aaAAbbBBccCCddDDeeEEffFFggGGhhHHiiIIjjJJkkKKllLLmmMMnnNNooOOppPP where: AAaa: Cell Voltage 1 BBbb: Cell Voltage 2 CCcc: DDdd: EEee: BAT Voltage. Voltage at the VC2 (BAT) terminal FFff: PACK Voltage GGgg: Cell Current 1. Simultaneous current measured during Cell Voltage1 measurement HHhh: Cell Current 2. Simultaneous current measured during Cell Voltage2 measurement IIii: JJjj: KKkk: Cell Power 1. Calculated using Cell Voltage1 and Cell Current 1 data LLll: Cell Power 2. Calculated using Cell Voltage2 and Cell Current 2 data MMmm: NNnn: OOoo: Power calculated by Voltage() × Current() PPpp: Average Power. Calculated by Voltage() × AverageCurrent() |