SLUUCT7B may 2023 – august 2023 BQ25756
The following list of equipment is recommended when testing with a constant voltage electronic load.
A power supply capable of supplying 40 V at 8 A is required. While this part can handle larger voltage and current, larger power levels are not necessary for this procedure.
Kikusui PLZ164WA 0-150V, 0-33A When testing without a real battery, connect 2000 uF of capacitance across the input.
Six Fluke 75 multimeters, (equivalent or better) or: Three equivalent voltage meters and three equivalent current meters.
A computer with at least one USB port and a USB cable.
Download and properly install bqStudio from https://www.ti.com/tool/BQSTUDIO.